Technical FAQs
Technical FAQs
StruxureOn Gateway 1.0.0 was tested on Microsoft Windows Server 2008 R2 SP1 and Server 2012 SP1. The application takes 225 MB of disk space and the server retains a maximum of 8 days of data, about 700 MB per day.
Set the screen resolution to at least 1024 x 768.
iPhone 4S and newer
iOS 8.0 and newer
Android 4.4 and newer
When you launch the StruxureOn Gateway, the browser might display a message that the connection is not secure. Since the application is installed on the local machine, the security certificate used by localhost is a self signed certificate. It is safe to add an exception to your browser for https://localhost.