Technical FAQs

Ask a Question

Video: How to place an ACRD200 unit into Standby or On

Issue:
How to put an ACRD200 unit into On or Standby

Product line: 
InRow Cooling Products ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:
 


First you need to access the On/Standby menu
 
Then select ENTER
 
You will be prompted for a Password if limited access is enabled
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Now you should be able to choose either On or Standby
 
Press ESC and now you should be able to change Limited access from No to Yes
 
Limited access set to yes will only allow users to turn unit On or Standby with correct password.
Was this helpful?
What can we do to improve the information ?