Can I use the Pod Sharing functionality of NetBotz devices with Scanned devices?
Issue:
Pod Sharing functionality of NetBotz devices with SNMP Scanned devicesnot an option.
Product Line:
NetBotz
StruxureWare Data Center Expert Environment:
Netbotz device crawlers or SNMPscanners.
Cause:
Scanned devices or Device Crawlers in older NetBotz appliances can not be used with the NetBotz pod sharing functionality.
Resolution:
It will be necessary to directly connect to the appliance that is monitoring the SNMP device to view this on a NetBotz web page or using Advanced View. StruxureWare DataCenter Expert can see this information.