Technical FAQs

Ask a Question

Details Returned from Powerware Devices via Netbotz Advanced Device Crawlers

Issue:

Details Returned from Powerware Devices via Netbotz Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Powerware UPS systems assuming the Powerware DDF (Device Definition File) is installed on the NetBotz appliance and the Powerware UPS is SNMP enabled. Please note that not all information listed below is available on all Powerware models.

Resolution:

 
  • Vendor
  • Model
  • Battery Time Remaining
  • Battery Voltage
  • Battery Current
  • Battery Capacity
  • Battery Status
  • Battery Last Replaced Date
  • Input Frequency
  • Input Phases
  • Input Voltage Phase
  • Input Current Phase
  • Input Watts Phase
  • Input Source
  • Dual Input Status
  • Output Load
  • Output Frequency
  • Output Phases
  • Output Voltage Phase
  • Output Current Phase
  • Output Watts Phase
  • Output Source
  • Bypass Frequency
  • Bypass Phases
  • Bypass Voltage Phase
  • Ambient Temperature
  • Ambient Humidity
  • Remote Temperature
  • Remote Humidity
  • Dry Contact Sensor
  • Nominal Output Voltage
  • Nominal Input Voltage
  • Nominal Output Watts
  • Nominal Output Frequency
Was this helpful?
What can we do to improve the information ?