Technical FAQs

Ask a Question

Determining SSL Connection Information from the Netbotz Advanced View

Issue:
Determining SSL Connection Information from the Netbotz Advanced View

Product Line:

NetBotz

Environment:

NetBotz  version 2

Cause:

The Advanced View does not provide SSL session and connection information. To see the SSL session and cipher information, additional logging parameters must be configured.

Resolution:


Edit the "NetBotz Advanced View.lax" file in directory where the Advanced View is installed.
Add the following line to the file:
lax.nl.java.option.additional=-Djavax.net.debug=ssl

Save the file and restart the Advanced View.

Now the Advanced View Log file in the "logs" subdirectory will contain the SSL session information.

--------------------------------------------------------------------------------

Was this helpful?
What can we do to improve the information ?