Technical FAQs

Ask a Question

Which PDUs are used in the SmartBunker SX and CX?

Issue:
A customer is asking which PDU is included in the SmartBunker SX and CX. 

Product Line:
SmartBunker SX and CX

Environment: 
All versions and serial ranges.

Cause: 
Customers want to know which PDU comes with the SmartBunker SX or CX. 

Resolution:
PFMSB30024NA ships with AP7902. 
PFMSB30042NA ships with AP8958NA3. 
PFMSB40024NA ships with AP7902 and AP9567. 
PFSMB40038NA ships with AP8958NA3. 
Was this helpful?
What can we do to improve the information ?