Technical FAQs

Ask a Question

Why am I not able to establish communication with external batteries and my SURT15k/20K UPS?


Cannot establish communications with external battery packs

Product Line:

Smart-UPS Online


All SURT 15K and 20K models, All Serial Numbers


Communications are sometimes slow to initialize when connecting external battery packs.

  • Disconnect all external battery packs - Wait at least 2 minutes
  • Connect first battery pack - Wait at least 2 minutes
  • Connect next battery pack - Wait at least 2 minutes
  • Continue until all battery packs are recognized and communicating with the UPS. 

If issue persists, consult your users manual for additional troubleshooting methods.
Was this helpful?
What can we do to improve the information ?