Technical FAQs

Ask a Question

How do I reset my MGE NMC Password

MGE NMC Password reset
Product line:
66074 / 34003640SE MGE NMC
All Product models, all serial numbers
How do I reset my MGE NMC Password. Customer lost or does not know the default user name / password for web access to the NMC
The default user name / password are: MGEUPS (for both and must be in caps) If the issue requires an actual reset of values note that the card must be removed from its slot and we recommend the user place the UPS into bypass / maintenance bypass for this due to risk of operational state change if UPS is left online.
Refer to attached User Guide -
Was this helpful?
What can we do to improve the information ?