Technical FAQs

Ask a Question

Large device discoveries in StruxureWare may affect performance.


Discovering large numbers of nodes in StruxureWare Central or StruxureWare Data Center Expert can result in performance issues, sometimes requiring a system reboot.

Product Line:

StruxureWare Data Center Expert
StruxureWare Central
InfraStruxure Central


All current versions


Discoveries send larger amounts of data requests than normal scans. In many cases, other files such as configuration files and DDF files are also transferred during discovery


For best results, it is recommended that a large discovery job, for example 2000 SNMP devices, be run as several smaller discoveries.
Was this helpful?
What can we do to improve the information ?