Technical FAQs

Ask a Question

Netbotz Graph shows in Fahrenheit even though region settings suggest Celsius

Issue:

Netbotz Graph shows in Fahrenheit even though region settings suggest Celsius

Product Line:

NetBotz

Environment:

NetBotz version 3 appliances and graphing

Cause:

Although most translations are either based in the Advanced View software that pulls it's region information from the local computer or from the bot itself which has it's own region settings, the graph feature uses both the Advanced View and the Bot itself to pull this information. Since the local computer settings can differ from the Netbotz appliance settings, it was determined that the best alternative to having mixed languages and temperature readings was to have the graph read as English US.

Resolution:

Version 3.2 Botzware for Version 3 Netbotz products resolves this issue.
 
Was this helpful?
What can we do to improve the information ?