Technical FAQs

Ask a Question

When Exporting a report from ISX Central to view in Microsoft Excel using Chinese UI, some strange characters may exist.

Issue:
When Exporting a report from ISX Central using Chinese UI to view in Microsoft Excel, some strange characters may exist.

Product Line:
InfraStruxure Central

Environment:
InfraStruxure Central any version

Cause:
Configuration changes required in Excel

Resolution:
To view the export properly the user must do the following within Excel:
"Data" > "Import External Data" > "Import Data" > (select the file) "Open"

Then change the "File origin" to "936 : Chinese Simplified (GB2312)"

Was this helpful?
What can we do to improve the information ?