Wrong status if wrong sensor is plugged into sensor port on Netbotz Rack Monitor 550 with an Internal SP150
Issue:
Wrong status if wrong sensor is plugged into sensor port on Netbotz Rack Monitor 550 with an Internal SP150
Product Line:
NetBotz
Environment:
NetBotz version 3 appliances and sensors
Cause:
In some instances, sensors can be connected to only specific sensor ports.
Resolution:
"The attached XL sheet lists all the issues that may be seen if the wrong sensor is plugged into a port on the Netbotz 550.
This attachment references the following sensors:
Temp
Temp / humidity
Smoke
Vibration
0-5 volt cable
Spot leak
Rope Leak
Beacon
Dry contact
Ethernet
Door
A-Link
plugged into the following ports:
Universal Sensor port 1-6
Rope port
Beacon port
Ethernet port
A-Link port