Details Returned from DMTF Devices via Advanced Device Crawlers
Issue:
Details Returned from DMTF Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for DMTF systems assuming the DMTF DDF (Device Definition File) is installed on the NetBotz appliance and the DMTF system is SNMP enabled. Please note that not all information listed below is available on all DMTF models.