Details Returned from APC Devices via Advanced Device Crawlers
Issue:
Details Returned from APC Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for APC UPS systems assuming the APC DDF (Device Definition File) is installed on the NetBotz appliance and the APC UPS is SNMP enabled. Please note that not all information listed below is available on all APC models.