Technical FAQs

Ask a Question

What output voltage do I select when setting up a Smart-UPS SRT that supports multiple output voltages?


Issue:

What output voltage do I select when setting up a Smart-UPS SRT that supports multiple output voltages?

Product Line:

Smart-UPS Online

Environment:

SRT "LV" and "HV" Units - All Serial Numbers

Cause:

Some Smart-UPS SRT products will prompt you to select your output voltage during the initial Start-UP Wizard

Resolution:
 

In most applications you sould set the output voltage to match your nominal input voltage. (IE: If you are feeding your UPS 208v, set the output to 208v)
This will allow your UPS to feed the appropriate voltage to your equipment whether it is online or in bypass.

Was this helpful?
What can we do to improve the information ?