TFTPD32.exe no longer bundled in NetBotz firmware download
Issue:
TFTPD32.exe no longer bundled in NetBotz firmware download
Product Line:
NetBotz
Environment:
NetBotz firmware downloads 4.5.1 and after
Cause:
Some antivirus programs see TFTPD32.exe as a vulnerability. In all actuality, it is not however some vulnerabilities may include TFTPD32.exe in order to install themselves but antivirus programs such as McAffee point out that the file itself is not a virus:
http://home.mcafee.com/virusinfo/virusprofile.aspx?key=103882
Resolution:
Due to customer concern, we no longer provide this tftp program with our future downloads. The files used to update using this feature are still available in the download. If you have a tftp program available and wish to use this feature, feel free to do so. If you wish to download the tftpd32.exe program, it is available here:
http://tftpd32.jounin.net/tftpd32_download.html