Technical FAQs

Ask a Question

Is there a document available that shows which roof height adapters are used in various applications like EcoAisle and InRow?

Issue: 
There's a need to confirm the correct roof height adapter; that it's compatible with the product and application where it's being installed.  

Product Line:
InRow Cooling, NetShelter SX, NetShelter VX

Environment:
All versions and serial ranges.

Cause:
There are a few PDUs which don't have mounting holes for roof height adapters, and there is need to help choose the correct roof height adapter for a particular application.

Resolution:
See attached file

Was this helpful?
What can we do to improve the information ?