Technical FAQs

Ask a Question

How deep must the AR7580A Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?

Issue:
Need to make sure the cable cover opens far enough to install and maintain cables.

Product Line:
NetShelter SX
 
Environment:
All versions and serial ranges.
 
Cause:
Customer needs to be able to fully open the hinged cable cover to add, move or change cables.
 
Resolution:
The AR7580A cable manager needs to be installed at least 10.5" deep in order for the AR7581A hinged cover to open a full 90 degrees.
Also see attached file for photo.
Was this helpful?
What can we do to improve the information ?