Technical FAQs
Technical FAQs
Issue:
Ozone Depleting Chemicals
Product line:
All Cooling Units
Environment:
All Product models, all serial numbers
Cause:
Ozone Depleting Chemicals
Resolution:
AC Cooling equipment: ODC Ozone Depleting Chemicals
There is a push from the EPA to move away from ODC’s used in refrigeration. You may be asked, especially from Canada sites, if our systems use ODC. Our current 2012 line of cooling equipment do not use ODC. However, some of our older systems do use R22 which is considered an ODC.
Which units use R22?
AFX, CCT, CM, FM, ACPA4000, and TC all use R22 which is an ODC
What other refrigerants do we use that are not ODC?
410a
ACPSCx, ACRD10x, ACSC10x, TDVAx
407c
ACRP10x, ACRD50x, ACPDX21-86
134a
RDU, OA,