Technical FAQs

Ask a Question

PowerChute Business Edition: Security Alert when “Launching programs and files in an IFRAME” in IE is disabled.

Issue:
Security Alert when “Launching programs and files in an IFRAME” in Internet Explore has been disabled.

Product:
PowerChute Business Edition

Environment:
Windows Internet Explore

Cause:
“Launching programs and files in an IFRAME”  has been disabled

Solution:

If “Launching programs and files in an IFRAME” is disabled in Internet Explorer, a Security Alert is displayed when you try to log on to PowerChute Business Edition Agent.
If “Launching programs and files in an IFRAME” is disabled, enable it. For Internet Explorer 9.0, you enable it as follows:
1)     Select Internet Options on the Tools menu in Internet Explorer.
2)     On the Security tab, open the list of custom level settings.
3)     Under Miscellaneous, enable “launching programs and files in an IFRAME.
Was this helpful?
What can we do to improve the information ?