Technical FAQs

Ask a Question

Output relay state upon boot up of a Netbotz version 3 appliance.

Issue:

Output relay state upon boot up of a Netbotz version 3 appliance.

Product Line:

NetBotz

Environment:

Netbotz Version 3 output relay.

Cause:

Relays have a default state defined at startup. This is defined for factory defined switches and buttons as well as for custom created switches and buttons. Upon a reboot of the Netbotz appliance, the relays will go back to their default state. If there is an alert that is configured to trigger a state change on one of these buttons or switches, the state will then change as configured.

Resolution:

This is working s designed.

Was this helpful?
What can we do to improve the information ?