FTP Alert Action in Version 2 Appliances is Active Mode Only
Issue:
FTP Alert Action in Version 2 Appliances is Active Mode Only
Product Line:
NetBotz
Environment:
NetBotz version 2 and 3
Cause:
The FTP Alert Action included with the Version 2 Appliances (320, 420, 500) is an Active Mode FTP session only. At this time, NetBotz Appliances do NOT support passive FTP.
Resolution:
This is by design. No alternative options are available.