Technical FAQs

Ask a Question

Adding Additional Door Switch Sensors to a version 2 NetBotz appliance

Issue:

Adding Additional Door Switch Sensors to a version 2 NetBotz appliance

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

Optional configurations

Resolution:

NetBotz sells additional door sensors that plug into the external sensor DIN ports. The DIN connector door sensor can be attached to any NetBotz monitoring appliance that supports DIN connector style sensors. The NetBotz appliance can support as many door switch sensors as it has DIN connector ports.

Was this helpful?
What can we do to improve the information ?