Replace Battery
Replace the internal battery soon.
Contact Conext. Like car batteries,
back up batteries last an average
of 3 to 6 years.
AVR
Automatic Voltage Regulation provides
better runtime and longer battery life.
7 Surge Protected Outlets
All outlets protect against lightning, surges and spikes.
4 Battery Powered Outlets with Surge Protection
Supplies back up power to 4 outlets.
Room for 2 Block Adapter
Room for 2 transformer blocks (for external drives,
speakers, or printers) without blocking other outlets.
Telephone Line Protection
Protect your modem, telephone, or fax from
surges and spikes.
USB Data Link
Conext Shutdown Manager
Building Wiring Fault
If on, indicates something is wrong with your
building or outlet wiring, call an electrician.
Circuit Breaker
Just push in the button to reset.
Overload Alarm - continuous tone
Sounds when you have too much equipment
attached to the four battery back up outlets.
On Battery Alarm - 4 beeps every 30 seconds
Sounds when you are running on back up power.
Low Battery Alarm - continuous beeps
Sounds when battery runtime is almost depleted.
Save your files and shut down.