Technical FAQs

Ask a Question

What are the capabilities of the condensate pump on the ACSC unit?

Issue:
What are the capabilities of the condensate pump?
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
The pump can remove 1.3 gal/hr (5.9 l/hr) at a maximum run of 50 ft (15.2 m) of which 16 ft (4.9 m) can be vertical lift. For example, if you have 10 feet (3 m) of vertical lift, you have 40 feet (12.2 m) left for usable horizontal run.
Was this helpful?
What can we do to improve the information ?