Video: How to change the Maintenance Intervals on a Network Air FM unit
Issue:
How to change the Maintenance Intervals on a Network Air FM unit
Product line:
FM35-50, ACFM, IR40
Environment:
All Serial Numbers
Cause:
Install Operation
Resolution:
How to change the Maintenance Intervals on a Network Air FM unit follow the below procedures
1 Press ESC until you reach the main menu (On/Off)
2 Scroll to SETUP and press ENTER
3 Scroll to SYSTEM 1 and press ENTER
4 Press ENTER on ALARMS.
5 Press ENTER on MAINT ALARMS
6 Press ENTER to scroll through the device available
1 of 7 Compressors 1
2of 7 Compressor 2
3 of 7 Heaters
4 of 7 Blowers 1
5 of 7 Blowers 2
6 of 7 VFD 1
7 of 7 VFD 2
7 Press ENTER on the selected device
8 Press the DOWN arrow once then press ENTER again
9 Using the UP or DOWN arrows you can select the desired interval or disable this feature.