Technical FAQs

Ask a Question

Why does PowerChute Network Shutdown not start after upgrading system Java?

Issue:
After upgrading system Java PowerChute Network Shutdown web interface is not accessible.

Product:
PowerChute Network Shutdown versions 3.x & 4.x

Environment:
All supported OS

Cause:
When upgrading Java in most cases the older version in uninstalled so the path PowerChute uses to access Java no longer exist.

Solution:
Run the PowerChute installer which will discover the new path.
 
Was this helpful?
What can we do to improve the information ?