Video: Total Power Off Procedure for All Single Phase Symmetra Units
Issue
Proper procedure for powering down a single phase Symmetra
Product Line
Symmetra LX, Symmetra RM, Symmetra Power Array
Environment
All Single Phase Symmetra
Cause/Overview
There are times when it may be required to power down the Symmetra. Such instances could be to change out a system fan depending on the type of Symmetra, or changing out a backplate.
Resolution
The total power off procedure for Symmetra systems are found on the back of all of the systems.
The procedure is as follows:
1. Set the System enable Switch to Standby
2. Set the Input Circuit Breaker to Standby
3. Disconnect the Battery Modules
4. Disconnect external Battery Cabinet (if provided)
5. Disconnect Mains/Branch Circuit