Technical FAQs

Ask a Question

How many leak sensor cables can be attached in series on an 600 mm unit

Issue:  How many leak sensor cables can be attached in series on an 600 mm unit

 

Product line: All InRow 600 mm units

 

Environment:  All Serials

 

 

Cause:  Install

  

 

Resolution:

 

 

Leak sensor

 

Install up to four optional leak sensors (AP9326) as needed. 1. Connect the leak sensor to the equipment using the plug located as shown.

 

Position the leak sensor inside or outside the equipment.

 

 

 

Route the leak sensor to the outside of the equipment through either the bottom plate or the door.

 

Secure the leak sensor wire to surfaces using cable ties and cable tie holders (provided with the leak detector).

 

 

 

 

 

 

 

Was this helpful?
What can we do to improve the information ?