Technical FAQs

Ask a Question

Uniflair BACnet (Building Automation and Control Networks)

 
                                                                                                                                                         

Issue:  Uniflair BACnet (Building Automation and Control Networks)

 

Product line: Uniflair

 

Environment: All Models and Serial Numbers

 

 

Cause: Install

  

 

Resolution:  

 

scheda seriale 485      Gateway

 

All the units must be fitted with a RS485 card, trough that they are connected to the RS485 serial cable. On one side there will be the 120 ohm resistor, on the other, the gateway which will translate the variables from Uniflair language, to LON language.

 

To realize a local net to be connected to a BMS with protocol BACnet, it’s necessary:

• gateway LBM every 8 units; (not necessary with pCOnet - pCOWeb)

• 1 RS485 serial card for every controller;

• 120Ω resistor;

• PC for the gateway configuration

 

BACnet is a supervisory system created from AHRAE:

“American society of Heating, refrigerating and Air conditioning Engineers”

These are the ways how the information under BACnet can be sent to Uniflair controllers:

 

    BACnet IP/Ethernet

 

 

1111    pCOnet:  connessione RS485

 

 

 

Gateway   Gateway

Carel :

  1. Protocol Carel
  2. Connection RS485 or RS422
  3. Max 8 units
  4. No software modification needed

BACnet :

  1. BACnet PTP
  2. Connection RS232
Was this helpful?
What can we do to improve the information ?