Technical FAQs

Ask a Question

InRow: What is capacity regulation?

What is capacity regulation?

Product line: 
ACRD100, ACSC100

All versions and serial numbers.

Configuration & Installation

Capacity regulation is a method of controlling the capacity of the InRow RD unit. This is achieved using an electronic Hot Gas Bypass Valve (HGBV) which allows the unit to operate at low load conditions down to 2.5KW without compressor recycling.


Was this helpful?
What can we do to improve the information ?