Technical FAQs

Ask a Question

What is the flow rate required for the InRow ACRD2XX fluid-cooled unit?

Issue:
What is the flow rate required for the InRow ACRD2XX fluid-cooled unit?

Product line:
ACRD2XX

Environment:
All systems.

Cause:
Normal operation and configuration.

Resolution:
Each InRow RD fluid-cooled unit requires a flow rate of 10gpm within its loop. This is for a single RD piped to a single outdoor fluid cooler. The flow rates will vary for custom configurations consisting of multiple RD units to a single outdoor dry cooler. Additional guidance on flow rates can be obtained from the Applications Engineering team.

 

 
Was this helpful?
What can we do to improve the information ?