Technical FAQs

Ask a Question

StruxureWare Central's Web client ignores US/Metric units setting.

Issue:
StruxureWare Central's Web client ignores US/Metric units setting

Product Line:
StruxureWare Central / Data Center Expert

Environment:
StruxureWare Central / Data Center Expert potentially any version prior to 7.2

Cause:
If the server locale is set to anything other than English US, The StruxureWare's web client ignores the selection of US Units so that values show up as Celsius rather than Fahrenheit.

Resolution:
This issue is resolved on StruxureWare Data Center Expert version 7.2
 
Was this helpful?
What can we do to improve the information ?