Technical FAQs

Ask a Question

Length of the Netbotz Audio-Style Door Sensor

Issue:

Length of the Netbotz Audio-Style Door Sensors

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2.

Cause:

Cable length

Resolution:

An appliance (NetBotz 500/420/320/400/310 series) comes with a door sensor that plugs to Switch Sense port(an audio-style connector). Length of the door sensor depends on the appliance is a 'rack' or 'wall' unit.

A NetBotz rack-mount appliance comes with a 12-ft door sensor; a NetBotz wall-mount appliance comes with a 50-ft door sensor.

There is also DIN-style door sensor (12-ft) available for purchase. It is for used with an external port on a Sensor Pod 120 or a NetBotz appliance.

Door sensor for additional cameras:

A Camera Pod 120 (purchased separately from an appliance) comes with a 50-ft door sensor. However, a CCTV Adaptor Pod 120 does NOT come with a door sensor. Separate purchase is required.
Was this helpful?
What can we do to improve the information ?