Contents of the Mounting Kit Included with the Models 320 & 420
Issue:
Contents of the Mounting Kit Included with the Models 320 & 420
Product Line:
NetBotz
Environment:
NetBotz 320 & 420
Cause:
N/A
Resolution:
The following items are included in the mounting kits:
Black universal swivel wall mount (plastic)
3 anchors (1"" long)(suitable for concrete) and 3 anchors (1-1/2"" long)(for sheet rock).
4 screws (#6 x 1/4"", phillips)
5 black tie wraps (7-1/2"" long) and 4 platforms (adhesive; can be stuck on walls; used with the tie wraps).