SNMP OIDs required for Rack PDU 2G products - which are correct?
Product Line:
Rack Power Distribution 2G products
AP88XX Metered Rack PDU 2G
AP89XX Switched Rack PDU 2G
AP86XX Switched Rack PDU with Metering By Outlet
AP84XX Metered by Outlet Rack PDU
Environment:
All serial numbers
All firmware versions
Users utilizing SNMP for polling
Cause:
APC's Next Generation Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX) utilize a separate MIB subtree for querying values via SNMP. These devices are able to report voltage, amps, volts, kW, and kWh, rather than just amps like their predecessors.
Resolution:
In order to query any Rack PDU 2G units via SNMP, the subtree is located at that the following OID: