Is the AR7731 compatible with NetShelter SV cabinets?
Issue:
Customers want to close off all open spaces on a NetShelter SV cabinet.
Product Line:
NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The Compatibility Chart shows that the AR7731 is not compatible with the NetShelter SV cabinets.
Resolution:
The AR7731 is designed for use with the NetShelter SX. In the kit, the strips that are used to close off the space between the cabinet and the floor are too short.
You can stack these pieces atop one another to create a taller strip.