Technical FAQs

Ask a Question

Is there a roof fan available for the NetShelter SV cabinets?

Issue:
There does not appear to be an optional roof fan for the NetShelter SV cabinets.

Product Line:
NetShelter SV

Environment:
All versions and serial ranges.

Cause:
Some customers may want to add a roof fan to their NetShelter SV.

Resolution:
The NetShelter SV cabinets do not currently have roof fans available.
Some of the fans that can be used inside the SV cabinet are: ACF001, ACF002, ACF003, ACAC40001, ACF201BLK, ACF202BLK.

Was this helpful?
What can we do to improve the information ?