Technical FAQs

Ask a Question

Video: How do I configure StruxureWare Data Center Expert to send e-mail notifications?

StruxureWare does not email when a device goes into alarm.

Product line:
StruxureWare Data Center Expert

Version 6.3 to 7.x

For StruxureWare Data Center Expert to email out when a device is in alarm the follow option must be configured.

  1. The device (or manual threshold) must be associated to a Notification Policy
  2. The Notification Policy must have an Action Associated
  3. The Action must have the correct email address configured
  4. StruxureWare must be able to reach the email server

The following will explain how to test and configure email notification within StruxureWare Data Center Expert.


Enter and Testing Email Settings

  1. Test email setting by going to the Systems drop down menu located at the top of the client
  2. Select Server Administration settings
  3. Select Email settings
  4. Enter then test displayed settings by using the Test Email Settings icon.
  5. Enter a valid email address


Creating and test email actions

  1. Click on Alarm Configuration drop down menu
  2. Select Manager Alarm Action
  3. Select Create (to test an action jump to Step 9)
  4. Select Send E-Mail then Next
  5. Enter an Action Name
  6. Click Add
  7. Enter email address then click OK (repeat steps 6 & 7 to add multiple emails
  8. Click Finish
  9. Test the action by selecting the action then click Test


Associating an Action to a policy

  1. Click on the Alarm Configuration Icon between Surveillance and Report
  2. Located at the bottom left corner right click on Default then select Edit (if missing go to the Windows drop down menu and select Restore Default Screen Layout)
  3. Locate and click the Add icon to the right side of the window
  4. Select the action to be associated to the Notification Policy
  5. Choose notification option
  6. Click OK
  7. Select Choose Thresholds to verify which Thresholds will be associated to this Policy
  8. Click on the Device Tab to verify which devices are associated to this Policy
  9. Click OK


*Note: By default all Devices are added to the Default notification policy.  

Was this helpful?
What can we do to improve the information ?