Technical FAQs

Ask a Question

Are the NetShelter SX Cabinets grounded per UL / IEC 60950, 61010-1 / 6.5.1.3?

Issue:
Customers require information on grounding NetShelter cabinets to IEC specifications.

Product Line:
NetShelter SX
 
Environment:

All versions and serial ranges.
 
Cause:

This installation requires grounding per IEC specifications.
 
Resolution :

NetShelter SX cabinets are UL Listed and have all metal components grounded per UL/IEC 60950 requirements and meet the 0.1 ohm resistance.
Equipment to be installed in a NetShelter SX cabinet should be Listed equipment.
Installation of any unlisted or recognized components requires a safety review of the completed assembly.
Was this helpful?
What can we do to improve the information ?