Technical FAQs

Ask a Question

How deep must the AR7580A Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?

Need to make sure the cable cover opens far enough to install and maintain cables.

Product Line:
NetShelter SX
All versions and serial ranges.
Customer needs to be able to fully open the hinged cable cover to add, move or change cables.
The AR7580A cable manager needs to be installed at least 10.5" deep in order for the AR7581A hinged cover to open a full 90 degrees.
Also see attached file for photo.
Was this helpful?
What can we do to improve the information ?