Technical FAQs

Ask a Question

NetBotz CCTV Adaptor Pod 120 Does NOT Come with Door Sensor

Issue:

NetBotz CCTV Adaptor Pod 120 Does NOT Come with Door Sensor

Product Line:

NetBotz

Environment:

NetBotz CCTV camera pod NBPD0123.

Cause:
Included components

Resolution:

The magnetic door switch sensor (audio-style connector) does NOT come standard with the NetBotz CCTV Adapter Pod. This door switch is available separately from NetBotz. The part number for the door switch is NBDC0002.
Was this helpful?
What can we do to improve the information ?