Issue:
How Do you Clear an Airflow DG5 Alarm History?
Product line:
Airflow
Environment:
Data Center Cooling
Cause:
Resolution:
In order to clear the Alarm History you will need to follow the path below.
Path: Alarm History >> Blank Button >> Help
One you clear your alarms you do not need to cycle power the alarms should clear right away. The Microprocessor will track the last 20 alarm occurrences. Each occurrence is displayed as a list. Each list will store up to ten different alarms per time occurrence.
Caution: Once the history is cleared from memory, it is permanently lost and cannot be recalled. In some instances it may become desirable to clear the history from the controller.