BOTSWANA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
BOTSWANA - Choose Country or Region
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
NEMA 5-15 receptacle description
Issue:
Which terminal is which in a standard household outlet?
Product Line:
Smart-UPS, Back-UPS, Surge
Environment:
All models, All Serial Numbers
Cause:
Informational
Resolution:
The NEMA 5-15 receptacle is the most common electrical receptacle in the United
States and Canada. It is a two-pole, three-wire grounding receptacle which is
used for a maximum of 15A and 125V. The standard wire colors are green for
Ground and white for Neutral. The color of the Hot wire can vary depending on
the building's electrical scheme; most common colors for the Hot wire are black
and red. The individual prongs: Hot, Neutral & Ground are well differentiated
as indicated in the diagram below.