Technical FAQs

Ask a Question

InfraStruXure Automatic Transfer Switch with Power Distribution (ATS); Operation manual, how to operate


Issue:
InfraStruXure Automatic Transfer Switch with Power Distribution (ATS); Operation manual, how to operate
 
Product line:
ISX-GEN-ATS 400A-800A, 250A, 400A
 
Environment:
All Product models, all serial numbers
 
Cause:
This manual is intended for end-users of the InfraStruXure Automatic Transfer Switch with Power Distribution (ATS). It provides important safety warnings and instructions, an overview of the ATS components, a detailed discussion of the ATS display interface, instructions on how to add components to the ATS, product and warranty information, and technical specifications.
 
Resolution:
Follow steps in Operation Manual

Also fine Reference Manual attached
 
 

 
Was this helpful?
What can we do to improve the information ?