"BIOS is Already Bypass Error on Adapter 0." message when restoring a Data Center Expert Enterprise server
Issue:
"BIOS is Already Bypass Error on Adapter 0." error is displayed when imaging a StruxureWare Data Center Expert Enterprise server from the v7.2.6 restore.iso:
Product Line:
StruxureWare Data Center Expert
Environment:
StruxureWare Data Center Expert v7.2.6 Enterprise server
Cause:
This informational message indicates the adapter is already in Bypass Error mode, a normal part of the restore process.
Resolution:
The 0 exit code indicates the error is harmless and can be overlooked.