Version 2 NetBotz 0-5V sensor on Sensor Pod 120 reports double the actual voltage in Advanced View
Issue:
0-5V sensors connected to the NetBotz Sensor Pod 120 with the NetBotz 0-5V Sensor Cable (NBAC0231) report double the actual voltage in Botzware and the Advanced View.
Product Line:
NetBotz
Environment:
Advanced View v4.3 and 4.4
NetBotz 0-5V Cable (NBAC0231)
Cause:
Firmware updates affected the performance of the NetBotz 0-5V Cable (NBAC0231).