Resolution:
Capacity regulation is a method of controlling the capacity of the InRow RD unit. This is achieved using an electronic Hot Gas Bypass Valve (HGBV) which allows the unit to operate at low load conditions down to 2.5KW without compressor recycling.