Technical FAQs

Ask a Question

Custom Property columns do not carry over for a Report configured as type Summary with a Table Export

Issue:

Custom Property columns do not carry over for a Report configured as type Summary with a Table Export

Product Line:

StruxureWare Central/StruxureWare DataCenter Expert

Environment:

Upgrade from StruxureWare Central version 7.0 to StruxureWare DataCenter Expert version 7.2

Cause:

not Specified.

Resolution:

When upgrading from StruxureWare Central version 7.0 to StruxureWare DataCenter Expert version 7.2, Custom Property columns that you may have had in a summary report with a table export will not be retained. To resolve this, you will need to edit the report after the upgrade.
 
Was this helpful?
What can we do to improve the information ?