Cannot Restore an ISX Central Backup when a user has special characters in the login account password
Issue:
Cannot Restore an ISX Central Backup when a user has special characters in the login account password
Product Line:
InfraStruxure Central
Environment:
Version 5.1
Cause:
If you create a share on a remote system to use as a repository for an ISX Central 5.1 backup and the user account used to access that share has any special characters in their password, the restore of that backup will fail
Resolution:
To resolve this issue, either use a user that has a password without special characters or create one for this specific action and remove the user or change his password until needed again. This issue was resolved in 6.x.